GEX2563900SWE-00(NORDICS)

Technical Data of Electrical Control and Operating Devices

The switchgear panels have been designed on principle so as to permit manual operation.

The drive mechanisms of the individual switching devices can be equipped, depending on the specific customer‘s model, with additional electrical control and operating devices. These are defined in the switchgear-specific circuit diagram, refer to the switchgear documentation.

Component fitting options:

  • Motor-operated drive mechanism for the earthing switch control element

  • Blocking coil

    The blocking coil helps to prevent manual actuation of the earthing switch. If the supply voltage has failed or is shut off, all blocking coils are in blocked position.

  • Auxiliary switches

    Auxiliary switches are always actuated directly by the truck or by the switch shaft via an intermediate linkage. Their position always corresponds to that of the main contacts. The switching functions have been set in the factory according to the circuit diagram.

  • Micro-switches are used depending on the customized panel models.

Overview of rated supply voltages

 

Overview of rated supply voltages

Direct voltage DC

24 V

48 V

60 V

110 V

125 V

220 V

Alternating voltage AC

(110)/120 V

(220)/230 V

Power consumption

Device

Rated power consumption

DC approx. [W]

AC 50/60 Hz approx. [VA]

Blocking coil

12

Motor for earthing switch

150

Information about the power consumption of solenoids and the motor is available in the related user guides, for example EvoPact HVX and CVX.


Trucks

Electrical control and operating devices of trucks are described in the appropriate Technical Manuals, refer to the Reference documents:

  • Circuit breaker EvoPact HVX with 12–24 kV, Ir ≤ 2500 A, refer to the Technical Instruction (AGS 531301-01)

  • Disconnector truck EvoPact UTX/Metering truck EvoPact MTX up to 24 kV, refer to the Technical Instruction (AGS 531361-01)

  • Vacuum contactor CVX, refer to the Technical Instruction NTV 133

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.