GEX2563900SWE-00(NORDICS)

Padlocks (not Included in Scope of Supplies)

The bore holes are provided for padlock yokes of Ø 8 mm.

 

Figure 32
Cover flaps on ON/OFF pushbutton for the circuit breaker can be locked by means of a padlock (optional)

 

Figure 33
Mechanical lock-out of earthing switch via padlock

 

Figure 34
Manual switching ON of circuit breaker locked by padlock

 

Figure 35
Manual switching OFF of circuit breaker locked by padlock

 

Figure 36
Mechanical lock-out for shutter (same principle for left-hand and right-hand sides)

 

Figure 37
Interlock of truck (optional)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.