GEX2563900SWE-00(NORDICS)

Safety Precautions

Safety Rules

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. Refer to standards or local equivalent.
  • This EvoPacT HVX Vacuum Circuit Breaker (VCB) and the PIX equipment must only be installed and serviced by qualified electrical personnel.
  • Perform work only after reading and understanding all of the instructions contained in this guide.
  • Turn off all the power sources before working on or inside the equipment.
  • Turn off or trip the VCB and discharge the mechanism.
  • Always use a properly calibrated voltage sensing device to confirm power is off.
  • Use only Schneider Electric specific tools (operating crank, extraction table, and so on).
  • Check all devices, covers, and doors are in correct position before turning on the power.
  • Beware of potential hazards and carefully inspect the work area for tools and objects that may have been left inside the equipment.
  • Do not modify the mechanical or electrical parts.
  • Do not bypass the interlocks before operation.
  • Do not operate with protective barriers removed.
Failure to follow these instructions will result in death or serious injury.
NOTICE
HAZARD OF INAPPROPRIATE HANDLING OR STORAGE CONDITIONS
  • Comply with the handling rules and avoid causing any shocks to the device.
  • If the equipment is stored before its final installation, observe the storage conditions.
Failure to follow these instructions can result in equipment damage.

Cleaning Instructions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not use solvents or alcohol for cleaning the equipment.
  • Do not use high-pressure cleaner for cleaning the equipment.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.