GEX2563900SWE-00(NORDICS)

Panel Design

Figure 1
Feeder panel PIX 12 with circuit breaker truck EvoPact HVX (for rated currents ≤ 2500 A)

1

Low-voltage compartment

9

Earth bar

2

Circuit breaker truck EvoPact HVX

10

Current transformer

3

Front door

11

Cable connections

4

Earthing switch control element

12

Make-proof earthing switch

5

Voltage indicator

13

Shutter

6

Position indicator of earthing switch

14

Busbars

7

Cable compartment cover

15

Pressure relief flap of switching device compartment

8

Voltage transformer (optional)

   
NOTE: Image is for representation purpose. Actual color of component/product may differ from document.

Figure 2
Feeder panel with circuit breaker truck EvoPact HVX (for rated currents ≤ 2500 A)

1

Jack rings for transport harness

9

Voltage transformer (optional)

2

Busbars

10

Cable compartment cover

3

Pressure relief duct

11

Cable connection

4

Pressure relief flap of cable compartment

12

Circuit breaker truck EvoPact HVX

5

Earthing switch

13

Front door

6

Current transformer

14

Pressure relief flap of switching device compartment

7

Cable fastening

15

Door of low-voltage compartment

8

High-voltage cable

16

Pressure relief flap of busbar compartment

Figure 3
Panel with Internal Arc Classification (IAC)

1

Pressure relief duct

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.