GEX2563900SWE-00(NORDICS)

Ratings of the PIX Series

Switchgear Panel

PIX 12

PIX 17

PIX 24

Rated voltage Ur

12 kV

17.5 kV

24 kV

Rated lightning impulse withstand voltage Up

75 kV

95 kV

125 kV

Rated power frequency withstand voltage Ud

28 kV

38 kV

50 kV

Rated normal current Ir

Busbar

≤ 3150 A(1)

≤ 2500 A(1)

Circuit breaker

Vacuum contactor

200–400 A

Rated peak withstand current Ip(2)

≤ 100 kA

≤ 80 kA

Rated short-time current Ik(2)

≤ 31.5 kA

≤ 31.5 kA

Rated frequency fr

50/60 Hz

(1) Higher ratings for forced cooling can be provided on request.

(2) The short-circuit capability of the current transformers must be considered separately.

The applicable panel-specific technical data are indicated on the nameplate (refer to the Nameplate) and in the switchgear-specific documentation.

The technical data of the switching device (EvoPact HVX, UTX) are indicated on the nameplate and in the operating manual of the device concerned.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.