GEX2563900SWE-00(NORDICS)

Switching Earthing Switch OFF

Follow the below steps to switching OFF the earthing switch:

  1. Push the slide (Figure 55, 1) upwards and insert the control lever of the earthing switch with the lever rod pointing to the right (2).

  2. Turn the lever counterclockwise by approx. 95° (3).

  3. Check position indicator: It must indicate that the earthing switch is OFF (4). Remove the lever.

 

Figure 55
Switch earthing switch OFF

1

Press slide upwards

2

Insert the operating lever

3

Turn operating lever counterclockwise

4

Position indicator reads: earthing switch is OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.