GEX2563900SWE-00(NORDICS)

Phase Comparators

Phase comparators are optionally available and not included in the scope of supplies.

Check phase coincidence before connecting different supply lines for the first time.

Phase Comparators for VDS Systems

If IVIS is used, phase comparison can be performed by means of the phase comparator MS 100 (Figure 21). For more information, refer Voltage Detection Systems (VDS).

Figure 21
Phase comparator MS 100

Phase Comparator for VPIS System

This phase comparator may only be used for the VIPS system in Voltage Present Indicating System VPIS.

Rated voltage Ur [kV]

VPIS item number

5–7.2

AMT150384-01

10–24

AMT150384-02

Figure 22
Phase comparator for HR system (Type ORION 3.0, Horstmann GmbH)


Check the device before each operation:

  • Connect the two plugs of the phase comparator to the two connection points of a VPIS device (Figure 23).

  • The lamp must light up: The phase comparator is working properly.

Figure 23
No phase coincidence: indicator lights up


Checking phase coincidence of two panels:

  • Connect the plugs of the phase comparator to the same phase connection points of two different VPIS devices (panels) (Figure 24).

  • The indicator must not light up. If the phases do not coincide, check the cable connection and, if necessary, exchange.

  • After each operation, check the device once more (see item 1).

Figure 24
No phase coincidence: indicator lights up

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.