GEX2563900SWE-00(NORDICS)

Replacing Fuse of Voltage Transformer

Voltage transformer in feeder cable

  1. Switch ON the panel’s earthing switch.

  2. Remove cable compartment cover, refer to the Access to the Main Circuit Compartments and Access to the cable compartment, Installation Manual (GEX2564100SWE-00(NORDICS)).

  3. Pull fuse (Figure 66, item 3) carefully out of the clamping contact.

  4. Check contact surfaces for cleanness and, if necessary, clean, refer to the Cleaning.

  5. Insert new fuse.

  6. Remount cable compartment cover.

Voltage transformer on metering truck EvoPact MTX

Refer to the Operating Manual (AGS 531361-01).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?