GEX2563900SWE-00(NORDICS)

PowerLogic PD100

The PowerLogic PD100 measures the partial discharge signals broadcast on the MV network through a capacitive coupler. The measurement is performed 24 hours a day, 7 days a week. The PowerLogic PD100 sends relevant data through a wireless communication network (Zigbee PRO) to a Zigbee PRO concentrator.

The PowerLogic PD100 is designed to be installed in the cubicle and connected to all three phases of the Medium Voltage supply of the cubicle. The PowerLogic PD100 is connected via the same capacitive connection as the one used for the VDIS unit. The PowerLogic PD100 can use the existing capacitive interfaces provided that the capacitive value is between ­13 pF to 128 pF.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.