GEX2563900SWE-00(NORDICS)

Racking-In the Truck from Disconnected into Service Position

Follow the below steps to racking-in the truck from disconnected into service position:

  1. Open cover (Figure 44, 1) and insert crank (2).

  2. Turn crank clockwise (3) until the truck has been racked in. Remove crank.

  3. Check position of truck (Figure 45) through the inspection glass.

 

Figure 44

1

Open cover

2

Insert crank

3

Turn crank clockwise

 

Figure 45
Truck in service position

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.