GEX2563900SWE-00(NORDICS)

Auxiliary Products

WARNING
hazard of incorrect use of auxiliary products
  • Only use the following auxiliary products, which can be obtained from the manufacturer, for mounting or maintenance. The use of other auxiliary products is not admissible.
  • The auxiliary products must be handled properly and according to the safety data sheets of the auxiliary products.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Auxiliary product

Order number

Cleaning agent

S008152

Lubricant KL, 0.5 kg can

ST312-111-835

Liquid lubricant FL, 0.5 kg can

S008153

Repair paint, 500 g can, RAL 7044, silk-grey

S009 492

The auxiliary products are available from the manufacturer. The use of alternative auxiliary products is not permissible.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.