GEX2563900SWE-00(NORDICS)

Dimensions and Weights (Without Packaging)

For the precise panel dimensions, refer to the switchgear-specific documentation. These depend on:

  • The rated voltage

  • The rated normal current

  • The rated short-time current and

  • Additional equipment:

    • Busbar or fan attachments

    • Rear high voltage cable connection

Figure 14
Dimensions of PIX panels

a

Panel width

b

Panel height (depending on height of low-voltage compartment)

c

Height of low-voltage compartment

d

Panel height without low-voltage compartment and attachments

e

Panel depth

Figure 15
Dimensions of pressure relief duct and deflector

1

Pressure relief duct

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.