GEX2563900SWE-00(NORDICS)

Lubrication Instructions

WARNING
hazard of incorrect maintenance
  • Do not disassemble circuit-breakers and drives for lubrication.
  • Only approved lubricants may be used. Refer to Auxiliary products.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
hazard of incorrect maintenance
The following elements must not be lubricated:
  • Motor
  • Ball bearings
  • Auxiliary releases
  • Push switches
  • Blocking coils
  • Auxiliary switches
Failure to follow these instructions can result in injury or equipment damage.

Preparation

  • Remove truck from the panel, refer to the Access to the Main Circuit Compartments and Removing the circuit breaker from the panel, Installation Manual (GEX2564100SWE-00(NORDICS)).

  • To get access to the fixed contacts behind the shutters, use a shutter lift (Figure 63).

  • Handling of the shutter lift corresponds to that of standard trucks (Evopact HVX and EvoPact UTX).

  • Clean lubrication points using a lint-free cloth; use cleaning agent in case of serious contamination, refer to the Annex.

Figure 63
Shutter lift

For a panel width of 650 mm, refer item number ADM I25 125-01.

For panel width 800/1000 mm, refer item number ADM I25 126-01.

Lubrication

Points of lubrication

Lubricant

Lubrication procedure

Sliding contact surfaces

KL

Clean by means of lint-free cloth; use cleaning agent in case of serious contamination. Apply a thin and uniform film of lubricant.

All accessible friction points and sliding surfaces

KL

Clean lubricating points using a lintfree cloth or a soft paint-brush, if necessary using cleaning agent (use sparingly, just moisten points of lubrication). Apply a thin coat of lubricant (using e.g. a paintbrush).

Bearings and joints

FL

Pour drops of liquid lubricant (oil can, drip feed lubricator) into the bearing gap. Liquid lubricant gets between the bearing surfaces due to the capillary effect. In case of inaccessible lubrication points, use an extension tube or spray.

Figure 64
Points of lubrication/maintenance

1

Earthing switch operating mechanism

2

Earthing switch contacts

3

Fuse of voltage transformer (optional)

4

Tracks for truck

5

Shutter mechanism

6

Fixed contacts for the truck

7

Switching device (lubricate in accordance with lubricating instructions in the appropriate operating manual EvoPact HVX/UTX/MTX)

8

Trolley, handling: refer to the Operation Accessories

Once maintenance work is complete:

  • Remove all the tools and auxiliary equipment used.

  • Reinsert truck into the panel, refer to the Access to the Main Circuit Compartments and Inserting the circuit breaker into the panel, Installation Manual (GEX2564100SWE-00(NORDICS)).

  • Reposition covers, close doors and check switching functions, refer to the Commissioning, Installation Manual (GEX2564100SWE-00(NORDICS)).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.