GEX2563900SWE-00(NORDICS)

Racking-Out the Truck from Service into Disconnected Position

Follow the below steps to racking-out the truck from service into disconnected position:

  1. Open cover (Figure 46, 1) and insert crank (2).

  2. Turn crank counter-clockwise (3) until the truck has been racked out. Remove crank.

  3. Check position of truck (Figure 47) through the inspection glass.

 

Figure 46

1

Open cover

2

Insert crank

3

Turn crank counter-clockwise

 

Figure 47
Truck in disconnected position

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.