GEX2563900SWE-00(NORDICS)

Electromagnetic Interlocks (Optional)

Electromagnetic blocking coils can be used for inter-panel as well as intra-panel interlocks:

  • The circuit-breaker ON and OFF pushbuttons are blocked.

  • Manual actuation of the disconnector truck is blocked.

  • Manual actuation of the earthing switch is blocked.

WARNING
HAZARD OF IMPROPER OPERATION
Locking of the switchgear interlocking must be complete to avoid malfunctions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

NOTE:
  • In case of failure of the supply voltage, all electrical interlocks are in the ”locked” position. Measure: Re-establish supply voltage.

  • Note the purchase contract and the switchgear specific circuit diagram as regards the design of the interlocking systematics.

NOTICE
Hazard of incorrect operating conditions
If no blocking coils are being used for the locking devices, a mechanical lock-out with cylinder or U lock must be provided.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.