GEX2563900SWE-00(NORDICS)

Operation Accessories

NOTE: These accessories are supplied together with the panel. The panel may only be operated by means of these accessories.

Designation

Item no.

Illustration

Handle for opening and closing the front door

SEM101120-01

Double-bit key for the front door

SEM101137-01

Double-bit key for the low-voltage compartment

SEM101137-02

Crank to charge the circuit breaker’s energy-storing device

AGS H30498-01

Operating rod to switch the circuit breaker on and off

AGS H35446-01


         

         

Designation

To be used for:

Rated value

Connector design

Item no.

Illustration

Operating lever for earthing switch

Cable feeder

Short-circuit current ≤ 31.5 kA

square

AMT000223-08 (motorized)

square

AMT000223-09

Short-circuit current 31.5 kA

hexagonal

AMT000223-10

Busbar

Short-circuit current ≤ 31.5 kA

square

AMT000223-05

Short-circuit current 31.5 kA

hexagonal

AMT000223-07

Crank for truck

Truck EvoPact HVX/UTX/MTX

Rated current Ir < 2500 A

hexagonal

AGSH31601-01 (manual drive)

Truck EvoPact HVX/UTX

Rated current Ir ≥ 2500 A

square

AGSH32532-01

   

AGSH31674-01

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.