GEX2563900SWE-00(NORDICS)

Replacement of Components and Panels

The drive mechanisms, current transformers and voltage transformers as well as the testing and monitoring systems can be replaced if necessary. Also, entire panels can be replaced.

The following data on the nameplate are relevant for replacement of components or panels or in case of any queries, refer to the Ratings of the PIX Series:

  • Type designation

  • Serial number

  • Year of construction

Should you have any queries regarding replacement of components or panels, contact the manufacturer’s Service Center.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.