GEX2563900SWE-00(NORDICS)

Avoid Condensation

DANGER
HAZARD OF ELECTRICAL ARC, EXPLOSION, AND FIRE
Make sure that the switchgear is provided with sufficient heating performance during installation and/or inspection of to help prevent condensation on the panel.
Failure to follow these instructions will result in death or serious injury.

Check that the specified insulating level, the switchgear panel – especially its insulating components – must not be exposed to condensation.

Measures to take in case of condensation

  • Should condensation be detected in or on the panel, clean the panel in accordance with Cleaning.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.