GEX2563900SWE-00(NORDICS)

Transport Trolley for Circuit Breaker

Figure 65
Transport trolley for truck

1

Autonomous interlocking of the racked-in truck on the trolley

7

Positioning of unlocking bar to match various panel versions

2

Variable screw fastening of track

8

Tray for accessories (lever, keys, handle)

3

Positioning of track to adjust the various track widths

9

Lever to lock/unlock the transport trolley on the panel. Table of trolley is lifted or lowered.

4

Track

10

Unlocking bar. The truck is unlocked in the panel.

5

Interlocking with panel

11

Handles of trolley

6

Variable screw fastening of unlocking bar

12

Slide to unlock the truck from the trolley


Rated volt-age Ur of the panel [kV]

Panel width [mm]

Truck

Item number of trolley

≤ 12

650/800

EvoPact HVX/UTX/MTX and CVX

EIB AE1 148-01(1)

1000

EvoPact HVX/UTX (Ir = 2500 A)

EIB AE1 148-02

EvoPact HVX/UTX (Ir = 3150 A)

AGS C74 125-01

≤ 17.5

750

EvoPact HVX/UTX/MTX and CVX

EIB AE1 148-01(1)

1000

EvoPact HVX/UTX (Ir = 2500 A)

EIB AE1 148-02

EvoPact HVX/UTX (Ir = 3150 A)

AGS C74 125-01(1)

24

800

EvoPact HVX/UTX/MTX and CVX

EIB AE1 148-01(1)

1000

EvoPact HVX/UTX (Ir = 2500 A)

EIB AE1 148-02

(1) The trolley can be used for panel widths of 650, 750 and 800 mm.



Adjusting the track width

Follow the steps to adjusting the track width:

  1. Release three screws on each track (Figure 65, 2).

  2. Adjust the two tracks to the appropriate panel track width and check them. Remount the six screws.

  3. Adapt position of unlocking bar (10) also to the appropriate panel (same procedure).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.