GEX2563900SWE-00(NORDICS)

Panel Variants

The sub-chapters always show panel types with the appropriate basic equipment. Customized models with additional equipment are described in the switchgear-specific documentation.

Functional Overview

PIX has a comprehensive range of functions to suit all requirements for many applications.

The table below can be used to link requirements to functional units and gives basic information on the general composition of each unit.

Panel Architecture

Feeder

Bus coupler

Bus riser

Busbar metering & busbar earthing

Application

Line transformer generator

Line

Line transformer motor capacitor

Motor capacitor

Auxiliary transformer

Bus section coupler

Bus section riser

Voltage transformer

Earthing switch

Main device

Circuit breaker

Disconnector or fix copper bar

Circuit breaker

Contactor with fuse

Load break switch with fuse

Circuit breaker

Voltage transformer, disconnector or fix copper bar

Voltage transformer

Earthing switch

Type of device

EvoPact HVX

EvoPact UTX

EvoPact HVX

CVX

LTRI

EvoPact HVX

EvoPact MTX, UTX or copper bar

EvoPact MTX

Earthing switch

Panel function

Incomer

Direct incomer

Feeder

Bus sectioning

bb voltage metering

Busbar earthing

Panel name, code

F

F

F

FC
(PIX-M)

FS

BSC

BSR

BME

Single line diagram

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.