GEX2563900SWE-00(NORDICS)

Operating the Circuit Breaker Manually

Switching ON via the Operating Rod

Insert the operating rod into the right-hand guide of the front door and press it right to the back (Figure 40, 1). The circuit breaker is switched ON; the position indicator indicates ON (2).

The energy storing device can be charged again immediately after switching ON (by hand or by motor). If supply voltage is present, the energy storage device is charged automatically.

Switching OFF via the Operating Rod

Insert the operating rod into the left-hand guide of the front door and press it right to the back (Figure 41, 3). The circuit breaker is switched OFF. The position indicator indicates OFF (4).

 

Figure 40
Switching the circuit breaker ON via the operating rod

1

Operating rod

2

Position indicator reads: Circuit breaker ON

 

Figure 41
Switching the circuit breaker OFF via the operating rod

1

Operating rod

2

Position indicator reads: Circuit breaker OFF

Switching ON via Pushbutton (Optional)

Press the left-hand lever down (Figure 42, 1). To switch ON, press the black pushbutton (right-hand - 2). The circuit breaker is switched ON. The position indicator indicates ON (3).

The spring can be charged immediately after switching ON (by hand or by motor). If supply voltage is present, the spring is charged automatically.

Switching OFF via Pushbutton (Optional)

Press the left-hand lever down (Figure 43, 4). To switch OFF, press the red pushbutton (left-hand - 5). The circuit breaker is switched OFF. The position indicator indicates OFF (6).

 

Figure 42
Switching circuit breaker ON via pushbutton

1

Press lever down

2

Press pushbutton I

3

Position indicator reads: Circuit breaker ON

 

Figure 43
Switching circuit breaker OFF via pushbutton

1

Press lever down

2

Press pushbutton O

3

Position indicator reads: Circuit breaker OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.