GEX2563900SWE-00(NORDICS)

Switching ON the Earthing Switch

Follow the below steps to switching ON the earthing switch:

  1. Push the slide (Figure 54, 1) upwards and insert the control lever of the earthing switch with the lever rod pointing upwards (2).

  2. Turn the lever clockwise by approx. 95° (3).

  3. Check position indicator. It must indicate that the earthing switch is ON (4). Remove the lever.

 

Figure 54
Switch earthing switch ON

1

Push slide upwards

2

Insert the operating lever

3

Turn operating lever clockwise

4

Position indicator reads: Earthing switch is turned ON

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.