GEX2563900SWE-00(NORDICS)

Earthing the Busbar with the Circuit Breaker of a Feeder Panel

The earthing device can be connected to a free cable terminal in the cable compartment access, refer to the Access to the Main Circuit Compartments and Access to the cable compartment, Installation Manual
(GEX2564100SWE-00(NORDICS)). If necessary, remove cable. The earthing device and the earthing adapter are not included in the scope of supplies.

NOTICE
hazard of incorrect operation
Comply with the specifications of the manufacturer of the earthing device and, if applicable, the earthing adapter.
Failure to follow these instructions can result in equipment damage.

Initial situation:

  • Feeder cable: OFF

  • Earthing switch: ON

  • Circuit breaker: OFF

  • EvoPact HVX truck: in disconnected position


Earthing the busbar

Follow the below steps to earthing the busbar:

  1. Connect the earthing device to the cable compartment (Figure 60, 1).

  2. Switch the earthing switch OFF (2).

  3. Move the truck to the service position (3).

  4. Switch circuit breaker ON (4).

Figure 60
Earthing the busbar with the circuit breaker of an feeder panel


De-earthing:

Follow the below steps to de-earthing the busbar:

  1. Switch circuit breaker OFF.

  2. Move the truck to the disconnected position.

  3. Switch the earthing switch ON.

  4. Remove the earthing device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.