GEX2563900SWE-00(NORDICS)

Nameplate

The type designation on the nameplates on the front of the panels (refer to Figure 16) informs about essential technical data. When submitting enquiries to the manufacturer or ordering spare parts, the following information is required:

  • Type designation

  • Serial number

  • Year of construction

Figure 16
Nameplate on panel front

A

Type designation

B

Serial number

C

Year of construction

D

Technical data

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.