GEX2563900SWE-00(NORDICS)

Operator Interfaces of Panels

Figure 25
Operator interface of PIX panels (shown in conjunction with the circuit breaker EvoPact HVX)

1

Lock to open and close the door of the low-voltage compartment

9

Lock permitting locking and unlocking of the front door

2

Protection and control device

10

Knob for releasing the opening for racking the truck in/out manually

3

Circuit breaker ON

11

Opening for racking the truck in/out manually

4

Circuit breaker OFF

12

Earthing switch operating element

5

Insertion opening for handle to open and close the front door

13

Voltage indicator

6

Inspection glass for indications and position of the circuit breaker

14

Position indicator of earthing switch

7

Knob for releasing the opening, for manual charging of the circuit breaker’s energy storing device

15

Securing bolts of the cable compartment cover

8

Opening for manual charging of the circuit breaker’s energy storing device

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.