GEX2563900SWE-00(NORDICS)

Utilization in Line with the Intended Purpose

PIX series air-insulated medium-voltage switchgear units are designed exclusively for switching and distributing electrical power. They may only be used in the scope of the specified standards and the switchgear-specific technical data. Any other utilization constitutes improper use and may result in dangers or damage of equipment.


WARNING
HAZARD of incorrect assembly, use and operation
  • Only use the PIX series air-insulated medium-voltage switchgear units in the scope of the specified standards and the switchgear-specific technical data.
  • Operate the PIX series air-insulated medium-voltage switchgear unit according to its intended use.
  • Assemble, connect or operate the PIX series air-insulated medium-voltage switchgear unit properly.
  • Use accessories or spare parts which have been approved by the manufacturer.
  • Do not convert the switchgear or attach inadmissible parts without the manufacturer’s approval.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.