NNZ6555700-01

HMI User Interface

The PowerLogic™ DVR unit is provided with a touch control panel to monitor the status of the system.

The PowerLogic™ DVR system operation is controlled online. Depending on the status of the system, the PowerLogic™ DVR system operates in different modes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?