NNZ6555700-01

Events Menu

The Events menu displays the active alarms in the system. The information displayed in this menu is used to detect problems in the installation and to take actions accordingly.

In the event of any detected failure, the Events menu displays the information of the event which is used by the technical personnel to analyse the problem. If any event occurs in the system, the bell icon on the lower left side will turn red.

Each system event has the following information:

  • Event code

  • Event name

  • Date and time of the event occurred

More information about each possible events that generates the fault in the system is provided in the section Troubleshooting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?