NNZ6555700-01

Manual Bypass Operation Mode

The PowerLogic™ DVR system consists of manual bypass switches that enable the maintenance work without interrupting the electrical power supply to the load. In this mode, the loads are not protected against the disturbances caused due to the electrical power supply.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?