NNZ6555700-01

Standards

The PowerLogic™ DVR systems comply with the following standards:

Regulation

Standard

Objective

European low voltage directive (2014/35/EU)

IEC 62477-1:2012/A11:2014

Safety requirements for power electronic converter systems and equipment

UK Regulation for Electrical Equipment (SI 2016 No.1101)

IEC 62477-1:2012/A11:2014

Electrical equipment to comply with Electrical Equipment (Safety) Regulations 2016

European directive on electromagnetic compatibility (2014/30/EU)

  • IEC 61000-6-2:2005: Immunity

  • IEC 61000-6-4:2007/A1:2010: Emission

Electromagnetic compatibility requirements for industrial environments

Shock and Vibration for “Class 3M1 Equipment”

IEC 60721-3-3:2002

Classification of groups of environmental, parameters and their severities-Stationary use at weather protected locations

UKCA marking

Manufacturer:

Schneider Electric Industries SAS

35 Rue Joseph Monier

92500 Rueil-Malmaison

France


Importer:

Schneider Electric Limited

Stafford Park 5

Telford, TF3 3BL

United Kingdom

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?