NNZ6555700-01

Voltage and Overvoltage Regulation

The PowerLogic™ DVR responds quickly and accurately with slow and fast voltage regulations (within the continuous regulation of PowerLogic™ DVR system) caused by the load variations that arise in the power grid.

The PowerLogic™ DVR regulation capacity compensates overvoltage upto +20%.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?