NNZ6555700-01

Internal Architecture of PowerLogic DVR System

The PowerLogic™ DVR system consists of a transformer and a set of reversible rectifier and inverter. The following image details the internal architecture of the PowerLogic™ DVR system.

The system receives the energy directly from the line. This energy is used to compensate the defective or excess voltage at its input, independently for each phase, to generate the stable output (±1%).

The PowerLogic™ DVR system consists of:

  • Preload

  • Rectifier

  • Inverter

  • Static bypass

  • Booster transformer

  • Digital signal processor (DSP)

  • Input autotransformer

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?