NNZ6555700-01

Operation Procedures

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462, or applicable local standards.
  • The equipment must be installed and serviced only by qualified electrical personnel.
  • Do not exceed the maximum limits of device ratings.
  • Ground the equipment using the provided ground connecting point before turning on the power supply to the system.
  • Turn off the power supply before working on the system.
  • Once the power is turned off, wait for 3 minutes to allow the capacitors to discharge prior to opening the doors or removing the covers.
  • Always use a sensing device of proper rated voltage to confirm that the power is off.
  • Replace all devices, doors, and covers before turning on the power supply to the system.
  • Carefully inspect the interior for tools left behind before replacing the covers and closing the doors.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?