NNZ6555700-01

Rectifier and Inverter

The rectifier and the inverter module consists of power structure integrated with a control system based on a DSP, which is responsible to operate the unit with excellent reliability.

The rectifier and the inverter module is operated by Pulse Width Modification (PWM), which is combined with an advanced control system. For the rectifier module, the PWM unit supplies continuous voltage to the DC-link from the alternating input voltage and for the inverter module, the PWM unit supplies a low distortion sine waveform from the DC-link.

The information to control the rectifier and the inverter module is transmitted to the DSP.

The rectifier and the inverter module consists of a forced ventilation system that will be activated during the start-up of the module.

The temperature sensor of the rectifier and the inverter module disables its operation, if the temperature of the module increases above the pre-determined values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?