Parameters Menu
The Parameters menu allows to visualise and to modify the operating parameters of the PowerLogic™ DVR system. The submenus of Parameters menu can be accessed by clicking the navigation tree on the left side of the screen.
The bottom of the screen consists of various buttons, which are used to change the configuration status. The following table describes the buttons.
|
Button |
Action |
|---|---|
|
Allows to save the current Temporary configuration of the PowerLogic™ DVR system and establish it as the Active configuration of the system. |
|
|
Allows to return to the previous Active configuration that was saved. |
|
|
Allows to restore the original values of factory default settings and sets them in the Temporary configuration. Press the Save button to set these values as Active parameters. |
|
|
Allows to change the language of the control panel. The available languages are Spanish, English, and Chinese. |
|
|
Accepts the modification of the parameter. |
The Parameters menu consists of following submenus which are used to set the parameters and to monitor the internal operation of the PowerLogic™ DVR system.
System
This submenu displays the details of the generic system data. The following table details the parameters of the System submenu.
|
Parameter |
Description |
|---|---|
|
Description |
Description of the equipment |
|
Location |
Description of the geographic location of the equipment |
|
Contact |
E-mail of the person in charge of the equipment |
|
Date |
Internal date of the equipment |
|
Time Zone |
Time zone of system clock |
|
Language for notifications |
Language of the description column of the Event Log menu |
|
Backlight Timeout |
Time (in minutes) to shut down the display of the equipment |
|
Logout Timeout |
Time (in minutes) to automatically end the user session |
Passwords
This submenu allows to change the passwords.
The following table details the parameters of the Password submenu.
|
Parameter |
Description |
Default password |
|---|---|---|
|
Basic User Password |
Allows to change the password for Basic User (level 1). |
BASIC111 |
|
Advanced User Password |
Allows to change the password for Advanced User (level 2). |
ADVAN222 |
Enter the Current password corresponding to the Active Access level, then enter the New password. The format of New password should be 8 characters long, numbers or letters (upper or lower case).
After 3 unsuccessful retries, access will be blocked for 1 minute.
To change the password on another level, first click on Access Level at bottom of the display and follow the procedure described on page 23 to log on the expected level. Then, repeat the procedure above to change the default password.
DVR
This submenu displays the generic information of the PowerLogic™ DVR system.
The following table details the parameters of the DVR submenu.
|
Parameter |
Description |
|---|---|
|
Nominal AC Voltage (LL) |
Nominal voltage of the mains (phase to phase) |
|
Nominal sag |
Percentage of sag that the system is able to compensate |
|
Number of parallel units |
Number of equipment connected in parallel |
|
Nominal Frequency |
Installation nominal frequency |