NNZ6555700-01

Switching from Manual Bypass to Normal Mode

To switch the PowerLogic™ DVR system from Manual Bypass to Normal mode operation, perform the following steps:
  1. Replace all devices and carefully inspect the interior for tools left behind before replacing the covers.
  2. Set the internal switch I1 of the PowerLogic™ unit to ENABLE START position.
  3. Turn the manual bypass input switch I1 to ON position.
  4. Make sure that the PowerLogic™ DVR system is turned on and the system is in the Static Bypass mode on the control panel.
  5. Turn the manual bypass output switch I3 to ON position and then the manual bypass switch I2 to OFF position.
  6. Turn the LOCK KEY anticlockwise, and remove it from the lock.
  7. Insert the corresponding key into START KEY I4 of manual bypass cabinet, and turn the key clockwise to start the system. Check that the system is started on the control panel.
    Result: The PowerLogic™ DVR system is switched from Manual Bypass to Normal operation mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?