NNZ6555700-01

Static Bypass

During the system Stop event, the static bypass module isolates the system from the input line. The Stop event can be triggered manually or due to an internal fault resulting in short-circuit in the primary of the booster transformer. The module consists of an ultra-fast electronic bypass and a parallel contactor to perform a permanent static bypass.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?