NNZ6555700-01

Booster Transformer

This module isolates the system from the input line, when the defective or excess voltage is compensated to maintain the stable output voltage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?