Status and Events
A Status is a mode of operation of the system in any possible situation. An Event is a condition which must be met to force a status change.
Depending on the events or different situations which may occur, the system switches through different working status which are reflected in:
-
Event Log menu as Status change events
-
Status menu
-
Home menu
The following table provides the list of possible working status of the system. The system compensates only when the static bypass is off and the inverter module is on.
|
Status |
Description |
Status of internal modules |
|---|---|---|
|
OFF |
The system is stopped manually. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
The system is in Mains failure or Minimum Bus Voltage status. In this case, the system will be in OFF status until the conditions are removed. |
||
|
Pre-charging |
Transitory status until DC-link voltage reaches a value. The precharge contactor is closed. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Pre-ON |
Transitory status until the system checks it can start. The precharge contactor is open and the main contactor is closed. |
Static bypass ON Rectifier module ON Inverter module OFF |
|
ON |
The system is working in normal operation mode. |
Static bypass OFF Rectifier module ON Inverter module ON |
|
Pre-OFF |
Transitory status between any status and OFF status. The main contactor is open. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Overload |
The system has detected an Overload event. Once the condition is removed, the system switches to ON status. |
Static bypass ON Rectifier module ON Inverter module OFF |
|
Instantaneous voltage failure |
The system has detected an Instantaneous voltage failure event. Once the condition is removed, the system switches to ON status. |
Static bypass ON Rectifier module ON Inverter module OFF |
|
Mains failure |
The system has detected a Mains voltage failure and/or a PLL failure event. Once the condition is removed, the system will follow the start-up sequence automatically. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Minimum bus voltage |
The system has detected a Minimum bus voltage event. Once the condition is removed, the system will follow the start-up sequence automatically. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Maximum sag |
The system has detected an Output voltage integrator limitation event. Once the condition is removed, the system switches to ON status. |
Static bypass ON Rectifier module ON Inverter module OFF |
|
Driver alarm |
The system has detected a Driver alarm event. The system will autoreset. If this is repetitive, the system switches to the Driver failure status. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Maximum bus voltage alarm |
The system has detected a Maximum bus voltage event. The system will autoreset. If this is repetitive, the system will change to Maximum bus voltage failure status. |
Static bypass ON Rectifier module ON Inverter module OFF |
|
Pre-charging failure |
When DC-link voltage does not reach a value in the start-up sequence. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Capacitor voltage failure |
The system has detected a Maximum capacitor voltage event. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Maximum bus voltage failure |
The system has detected a Maximum bus voltage event repetitively, or once being on Pre-ON status. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Thermostat failure |
The system has detected a Thermostat failure event. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Driver failure |
The system has detected a Driver failure event. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Temperature failure |
The system has detected a High temperature alarm event. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Fuse failure/AC capacitor failure |
Transitory status between any status (except OFF status) and Fuse failure or AC capacitor failure status. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
Fuse failure |
Input fuse blown. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
|
AC capacitor failure |
Any AC power capacitor of rectifier/inverter module has lost its capacity. This status must be manually reset. |
Static bypass ON Rectifier module OFF Inverter module OFF |
The events occurred in the PowerLogic™ DVR system are recorded in Events or Event Log menus. More information about each possible events that generates the fault in the system is provided in the section Troubleshooting.