Switching from Normal to Manual Bypass Mode
Perform the following steps to switch the PowerLogic™ DVR system from Normal to Manual Bypass mode:
-
Insert the corresponding key into the Lock Key of manual bypass cabinet and turn the key clockwise. The key will remain blocked in this position.
Result: The system switches to the Static Bypass mode. Make sure that the system is stopped on the control panel.
-
Turn the manual bypass switch I2 to ON position, and then set the manual bypass output switch I3 to OFF position.
-
Turn the manual bypass input switch I1 to OFF position.
Result: The PowerLogic™ DVR system is switched from Normal to Manual Bypass mode.
The following image shows the schematic of manual bypass cabinet.
The following image shows the switch views of manual bypass cabinet.
Before removing any protective cover of master or slave units, perform the following steps:
-
Set the internal switch I1 of the PowerLogic™ unit to the DISABLE START position.
-
Wait for at least 3 minutes for the capacitors to discharge.
-
Use a sensing device of proper rated voltage to confirm that the power is off.