Status Menu
The Status menu displays the general information about the status of the system.
The Status menu consists of the following submenus which are described in the following subsections. They can be accessed by clicking the navigation tree on the left side of the window.
System
This submenu displays the generic system data. The following table details the parameters of the System submenu.
|
Parameter |
Description |
|---|---|
|
Name |
Name of the equipment |
|
Description |
Description of the equipment |
|
Location |
Description of the geographic location of the equipment |
|
Contact |
E-mail of the person in charge of the equipment |
|
Code |
Code of the system (factory setting) |
|
Firmware |
Firmware version (factory setting) |
|
Configuration |
Status of the system configuration:
|
The Console Reboot button resets the screen without interrupting the equipment.
Measures
This submenu displays the PowerLogic™ DVR system measurements such as voltage, current, and power as shown in the following image.
The following table details the parameters of the Measures submenu.
|
Parameter |
Description |
|---|---|
|
Phase R Input voltage |
Input voltage phase R |
|
Phase S Input voltage |
Input voltage phase S |
|
Phase T Input voltage |
Input voltage phase T |
|
Bus Voltage |
Bus voltage |
|
Phase R Output voltage |
Output voltage phase R |
|
Phase S Output voltage |
Output voltage phase S |
|
Phase T Output voltage |
Output voltage phase T |
|
Phase R Output current |
Output current phase R |
|
Phase S Output current |
Output current phase S |
|
Phase T Output current |
Output current phase T |
|
Phase R Output power |
Output power phase R |
|
Phase S Output power |
Output power phase S |
|
Phase T Output power |
Output power phase T |
Status
This submenu displays the general system status.
The following table details the parameters of the Status submenu.
|
Parameter |
Description |
|---|---|
|
Control Status |
Working status of the PowerLogic™ DVR system (refer Status and Events) |
|
DSP Communication Failure |
Communication status between the control panel and the DSP:
|