NNZ6555700-01

Input Autotransformer (Only Used for AVC DVR 200/208/220 Vac Systems)

For PowerLogic™ DVR 200/208/220 Vac systems, an autotransformer is installed at the input of the rectifier.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?