NNZ6555700-01

Static Bypass Operation Mode

The PowerLogic™ DVR system sends a command to the static bypass and contactor to stop compensating the voltage during the following conditions, so that the output voltage is equal to the input voltage.

  • energized for the first time

  • stopped manually

  • stopped automatically due to a serious fault

  • the input voltage exceeds the tolerances allowed by the system

The system continuously analyses the grid input signal. The DSP helps to ensure the stability of the system as shown in the following image.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?