NNZ6555700-01

System Stop

To stop the system manually, perform the following steps:
  1. Insert the corresponding key into the Lock key of the manual bypass cabinet and turn the key clockwise.
    Result: This action sends the Stop command to the system. As a result, the system switches to the Static Bypass mode.
  2. Remove the Lock key from its lock. Turn the key anticlockwise to its initial position.
  3. De-energize the PowerLogic™ DVR system and the load.
  4. Turn the internal switch I1 of the PowerLogic™ DVR master unit to OFF position, and then switch I1 and I3 of manual bypass cabinet to OFF position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?