NNZ6555700-01

Menus

Once the PowerLogic™ DVR system starts, the Home screen appears on the control panel screen. By default, the screen displays the access level as Access Level: 1 (Basic User).

NOTE: The Access Level: 1 is a read-only access.

To edit the settings in the Parameters menu, the Access Level: 2 (Advanced User) is required.

To change the access level, perform the following steps:

  1. Press the Access Level button on the Status bar.

    Result: A Virtual keyboard appears on the screen.

  2. Select Level 2 and enter the default password: ADVAN222

    Result: The access level of the user is changed to Access Level: 2.

    NOTE: It is recommended to access the upper levels only by qualified technicians or Schneider Electric personnel.
  3. Pressing the Logout button on the Menu bar ends the current session.

    Result: The Home screen with Access Level: 1 is displayed.

The different menus are accessed from the Menu bar.

NOTE: If no operation is done on the control panel for 5 minutes (default), the screen saver mode is activated.

To activate the control panel, click on any part of the screen.

WARNING
Potential compromise of system availability, integrity, and confidentiality
Change default passwords at first use to help prevent unauthorized access to device settings and information.
Failure to follow this instruction can result in equipment damage.

For information on changing password, refer to Passwords menu on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?