General Precautions
Installation, wiring, testing, and service must be performed in accordance with all local and national electrical codes.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
For personnel and system safety, you must read and understand the instructions contained in this document before working on the system.
Keep these instructions in a place accessible to all the personnel who will work with the unit.
Arbitrary modifications are forbidden: The unit must not be subjected to any modification regarding its construction or safety without the consent from Schneider Electric. Schneider Electric will not own any responsibility for the damage caused as the result of the modification. Particularly, all repair work, soldering of printed circuit boards, and replacing of components, modules and printed circuit boards, without the authorisation from Schneider Electric is forbidden. Use only the original parts provided by Schneider Electric to replace the spare parts.
Use the unit for the purpose for which it was designed: Any other use of the unit is strictly forbidden. Schneider Electric is not responsible for any damage that might result when used for any other purpose. In such cases, the user shall assume exclusive responsibility for any risk. The use for which the unit was designed is defined in the documentation. The system shall be exposed only to admissible environmental conditions. These are defined in the technical details provided with the equipment.
Schneider Electric will not own responsibility for any inadequate, negligent, or incorrect installation of the equipment.
The instructions to operate the PowerLogic™ DVR system under safe conditions are as follows:
-
The system parts should not be used for other purposes.
-
The system does not contain any repairable or replaceable elements. In case of any malfunction or if any problem occurs while operating the unit, contact Schneider Electric.
-
Do not place the system near power magnets as this might cause a malfunction.
-
Do not block or cover the ventilation grills in the housing.
-
The system is designed in accordance with current EU legislation. Follow the electricity supply regulations corresponding to the country in which the unit is to be installed.
-
Even with all safety systems, verify that there is no voltage before touching any active point of the system.
-
The system is designed for industry use only. Do not use the system for domestic or commercial use.
-
During assembly work, start-up, or maintenance, it is recommended to wear personal safety equipment to avoid any damage due to accidental electric arcing.
-
The system must be protected against rain and excess humidity. It must be installed in a clean atmosphere where there is no inflammable liquids, gases or oxidising substances. If any liquid is spilt accidentally on the system, disconnect the system and consult Schneider Electric personnel immediately.
-
For any problems with the contents of this manual, contact Schneider Electric for assistance.
DANGER