NNZ6555700-01

Types of Disturbances

In addition to voltage sags elimination, the PowerLogic™ DVR topology also offers the possibility of mitigation of other energy quality problems at the same time such as fluctuations, Flicker effects, slow and fast regulation problems, and overvoltage and voltage unbalance.

The PowerLogic™ DVR has proven effective in mitigating the above energy quality problems with high stabilization accuracy and with an ultrafast response, generally less than 3 milliseconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?