NNZ6555700-01

Preload

During start-up, the preload module slowly increases the alternating input voltage to the rectifier. This module helps to prepare the equipment to start without drawing large current at the input.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?