NNZ6555700-01

Normal Operation Mode

During this mode, the rectifier and inverter modules will run and the static bypass module is open as shown in the following image. The output voltage is permanently regulated to the nominal voltage, if the input voltage and frequency are within the allowed range.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?