Home Menu
The Home menu displays the current status of the PowerLogic™ DVR system through synoptic scheme. It provides the visual information on status of different modules (such as transformer, static bypass, rectifier, and inverter), certain input and output measures, and the last registered sag.
The information about the last sag occurrence is displayed on left side of the window under Last Sag.
The Home menu displays the working status of the system (displayed below the inverter and rectifier blocks) as shown in the image.
The Home menu consists of the following buttons to perform the specific tasks.
|
Button |
Action |
|---|---|
|
Start |
This button is disabled because the start command is performed by the lock, which is placed in the manual bypass cabinet. |
|
Stop |
This button is disabled because the stop command is performed by the lock, which is placed in the manual bypass cabinet. |
|
Reset |
This button must be pressed when the PowerLogic™ DVR system stops due to an event which needs to be resolved. This button is used to restart the system. Pressing the Reset button will stop the PowerLogic™ DVR system, if it is working in the Normal mode. |